Technical FAQs

Ask a Question

How can Vijeo Citect v7.0 talk to my PLC using the TSXCUSBMBP USB to Modbus Plus adapter.

Currently, Vijeo Citect v7.0 does not have a driver to support the TSXCUSBMBP adapter. The workaround is to use the Vijeo Citect OPC driver and configuration the OFS configuration tool for the TSXCUSBMBP


Legacy KB System (APS) Data: RESL193042 V1.0, Originally authored by MiMe on 10/28/2008, Last Edited by MiMe on 10/28/2008
Related ranges: Vijeo Citect
Was this helpful?
What can we do to improve the information ?