Technical FAQs

Ask a Question

Which Citect product are not available under the Schneider offer?

Offically at this stage following PRODUCTS are Not Available under Vijeo Offer

1) Paging

2) Batch

3) Scheduler

4) Switch2Citect

5) CitectFacilities

As far as a technical reason goes it could be because default installation paths are diffrent for CitectSCADA and VijeoCitect and therefore project files can not be located in the expected directory

Vijeo path:
C:\Program Files\Schneider Electric\Vijeo Citect

Citect path:
C:\Program Files\Citect

Was this helpful?
What can we do to improve the information ?