Technical FAQs

Ask a Question

Is there a way to view all of my ProWORX NxT network page titles on the same logic screen?

Yes.
Viewing the network page titles on the same ProWORX NxT logic screen can be accomplished a couple of ways. Either clicking on "VIEW" then "NETWORK SUMMARY" or simply clicking on the "NETS" button will display this information.


Legacy KB System (APS) Data: RESL193034 V2.0, Originally authored by RoAl on 10/28/2008, Last Edited by RoAl on 01/26/2011
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?