Technical FAQs

Ask a Question

What is the frequency of the internal buzzer used in the Magelis XBTGT 2000 to 7000 series HMI terminals?


The buzzer frequency is between 2000Hz and 2600 Hz. (2300Hz typical)


Legacy KB System (APS) Data: RESL192877 V1.0, Originally authored by MiMe on 10/01/2008, Last Edited by MiMe on 10/01/2008
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?