Technical FAQs

Ask a Question

When I launch Vijeo Designer, I get an error message saying that Vijeo-Frame does not support Large Fonts. What could be causing this?


Vijeo-Designer error:

Your Display Properties are configured for Large Fonts.
Vijeo-Frame does not support this font mode.
If you continue the fonts and dialogs may appear incorrect.




Solution:

In the Display Properties dialog, there is a settings tab.
Goto that tab and press the Advanced button, you will see a new tab called General.
Please ensure that the DPI Setting is set to Normal 96 DPI.


Legacy KB System (APS) Data: RESL192874 V1.0, Originally authored by MiMe on 10/01/2008, Last Edited by MiMe on 10/01/2008
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?