Technical FAQs

Ask a Question

What is the purpose of the "Restore Project" feature in ProWORX 32?

The RESTORE PROJECT feature in ProWORX 32 is used if you want to restore a current project back to an older version of the same project that has been backed up. The older version of the original project would have to of been backed up as a .BAK file.


Legacy KB System (APS) Data: RESL192656 V3.0, Originally authored by RoAl on 08/30/2008, Last Edited by RoAl on 11/22/2012
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?