Technical FAQs

Ask a Question

What is the difference between a Micro 110CPU61200 and Micro 110CPU61204 controller?

There are two main differences.
The Micro 110CPU61200 has 2K logic memory words.
The Micro 110CPU61204 has 8K logic memory words and Comm port 2 supports XMIT Block Modbus Master.


Legacy KB System (APS) Data: RESL192647 V1.0, Originally authored by RoAl on 08/30/2008, Last Edited by RoAl on 08/30/2008
Related ranges: Modicon Micro
Was this helpful?
What can we do to improve the information ?