Technical FAQs

Ask a Question

CAN_HANDLER function block is missing in Unity Pro V4.0 Library MFB

Goals and Symptoms

CAN_HANDLER function block is missing in Unity Pro V4.0 Library MFB

Causes and Fixes

Now the CAN_HANDLER function block is hidden in the Unity Pro library. The customer doesn't have to instanciate it manually. Refer to the on-line help for more details and see attachment.

Was this helpful?
What can we do to improve the information ?