Technical FAQs

Ask a Question

Unity Pro V4.0 S and M: Failure to build new catalogs when using the Hardware Catalog Manager

Goals and Symptoms

When trying to build a new catalog, after adding a new device in the Hardware Catalog Manager under the Small and Medium packages of Unity Pro V4.0, an error occurs and the user gets this message: system cannot find the path specified.

Causes and Fixes

There is an issue with the installation of the S & M versions of Unity Pro V4.0; 2 directories are missing.
After installation, you will need to create 2 empty folders in the following path:
...\All Users\Application Data\Schneider Electric\ConfCatalog\UserCatalog\

The folders should be named as follows:

ToBeProcessed
Bmp

Depending on the installation, the path may vary. You can find it, however, in the registry base as shown in this image:




Once you create those two folders, you will be able to build the catalogs with no errors.

This issue is adressed in a Hotfix.


Legacy KB System (APS) Data: RESL192579 V1.0, Originally authored by MoAl on 08/25/2008, Last Edited by MoAl on 08/25/2008
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?