Technical FAQs

Ask a Question

XBTGT: How to connect XBTGT COM1 or COM2 to PC COM1 using Hyperterminal and ScriptDriver

Goals and Symptoms

XBTGT: How to connect XBTGT COM1 or COM2 to PC COM1 using Hyperterminal and ScriptDriver

Causes and Fixes

It is possible to successfully set up communication between HyperTerminal and the XBTGT 2130 on both of the target's COM ports.

Using COM1 is much simpler since no signal conversion is required and you can use standard Schneider cables.

COM2 is possible, but it requires creating two custom cables and using a converter to change the signal from RS-485 to RS-232.
Details for both setups can be found in the attached Word document and sample project.

Attachments

(Removed File URL: 192565_6432/hyperterm.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/ea39b0b9fbf73a50c12574b0003cadce/fl_block_5/0.4E8?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL192565 V1.0, Originally authored by DaBr on 08/25/2008, Last Edited by DaBr on 08/25/2008
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?