Technical FAQs

Ask a Question

Is there a replacement for the CER001 cable grounding clamp for Momentum Analog I/O modules ?

Yes, the replacement cable grounding clamp assembly has a part number of 170XTS16000. This clamp provides a secure grounding connection for the cable shields of the field wiring connecting the analog modules to the field devices. This clamp assembly mounts on a standard DIN rail and includes lock down screws. The use of this clamp assembly is recommended in systems that are required to meet CE compliance.


Legacy KB System (APS) Data: RESL192549 V1.0, Originally authored by DaSo on 08/20/2008, Last Edited by DaSo on 08/20/2008
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?