Technical FAQs

Ask a Question

Does the Advantys OTB configuration software have to be authorized ?

Advantys OTB configuration software does not have to be authorized. If you require the Advantys STB functionality, then it would have to be purchased and authorized. Starting with version 4.0 of the Advantys Configuration software, only online functionality with Advantys STB requires authorization.


Legacy KB System (APS) Data: RESL192436 V1.0, Originally authored by DaSo on 09/29/2008, Last Edited by DaSo on 09/29/2008
Related ranges: Advantys OTB
Was this helpful?
What can we do to improve the information ?