Technical FAQs

Ask a Question

What is the difference between the ASB553001 and the ASB553101?

The part number change reflects component changes necessitated by a vendor change. These changes do not affect customer functionality and there are no changes to the electrical specifications.


Legacy KB System (APS) Data: RESL192383 V2.0, Originally authored by DiSa on 07/25/2008, Last Edited by DiSa on 04/19/2010
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?