Technical FAQs

Ask a Question

How can I link symbols created in Proworx NXT into Vijeo Designer V4.6?


1 From ProWORX NXT project, go to "File -> Utilities -> Import/Export..."

2) In the "Import/Export Utilities" select "Export"

3) Select "Concept .TXT file"

4) Put in a path and filename so you can find your file.

5) Go to that directory and Rename the file *.CCN

6) In Vijeo-Designer project, make sure you have a Schneider EQUIPMENT driver added to the IO Manager

7) Right-click on the Variables node, and select "Link Variables..."

8) Go to the path of your renamed CCN file and select Files of Type: "Concept symbol export files (*.CCN).

9) Select your file and click Open.


Legacy KB System (APS) Data: RESL192228 V1.0, Originally authored by MiMe on 06/30/2008, Last Edited by MiMe on 06/30/2008
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?