Technical FAQs

Ask a Question

Why does ProWORX 32 always come up in Monitor Mode when I launch the software?

This is a setting found in the Environment Properties of ProWORX 32. If the option for "Start in Monitor Mode" is checked on, the ProWORX 32 software will always come up in Monitor Mode when launched. If you want ProWORX 32 to come up in Program Mode you must uncheck this option.


Legacy KB System (APS) Data: RESL192184 V1.0, Originally authored by RoAl on 06/21/2008, Last Edited by RoAl on 06/21/2008
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?