Technical FAQs

Ask a Question

Vijeo designer Lite limitation using chinese characters in alarm texts

Goals and Symptoms

Vijeo designer Lite limitation using chinese characters in alarm texts

Facts and Changes

With Vijeo Designer Lite : when using alarm history function with chinese character, It seems that chinese character cannot display properly. VDL converts alarm texts with chinese characters into ASCII texts.

Causes and Fixes

- The "Alarm panel" field must be filled with ASCII characters only, because usually this text is only used for alarm history printing.

- As XBTN/R/RT terminals support only text printers, so alarm text must always contain ASCII printable characters.
In other words, chinese texts need UNICODE characters, that is why the display under Vijeo-designer Lite appears only with ASCII characters (the original characters are converted by VD Lite into ASCII characters).

Morever, XBTRT500 doesn t support printing feature.
We advise you to recommand to the customer to use only ASCII characters.


Legacy KB System (APS) Data: RESL192143 V1.0, Originally authored by DaBr on 06/16/2008, Last Edited by DaBr on 06/16/2008
Related ranges: Vijeo Designer Lite
Was this helpful?
What can we do to improve the information ?