Technical FAQs

Ask a Question

Will the Concept .ASC file tell me what version of the firmware was in the PLC at the time of upload of the project?

No, to view the version of the firmware connect to the PLC with Concept, and go to <Online Control Panel>. The user can also view the version of the firmware in the PLC using the Concept Exec Loader and performing an Queery function.


Legacy KB System (APS) Data: RESL192037 V1.0, Originally authored by DaSo on 05/28/2008, Last Edited by DaSo on 05/28/2008
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?