Technical FAQs

Ask a Question

Search for a register only finds the coils used in the logic.

Goals and Symptoms

Search for a register only finds the coils used in the logic.

Facts and Changes

ProWORX 32 version 2.1B

Causes and Fixes

If you set the number for the 'End' parameter of the 'Network Range' in the 'Search' window to anything
greater than 5000 (i.e., 9999), location results for only the coils will be found. It does not return any location
results for the contacts. This only happens when the project is connected to the PLC in either the Online or
Combined mode. In some cases, the opposite behaviour may occur where only one of the contact
location will be found.


To resolve the problem, use a number that is less than 5000.
 


Legacy KB System (APS) Data: RESL191976 V1.0, Originally authored by AlCh on 05/23/2008, Last Edited by AlCh on 05/23/2008
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?