Technical FAQs

Ask a Question

Can the IP address for a M340 CPU or NOE be dynamically changed from a remote PLC as in a Premium PLC.

Goals and Symptoms

How can the IP address of the 'M340' CPU or NOE module be changed dynamically from a Premium

Facts and Changes

M340 PLC's

Causes and Fixes

No,you cannot use an application to change the IP address of a CPU or Ethernet port in an M340 as you can
in a Premium. The reason is because the M340 has limited functionality and does not support the SEND_REQ
block which would be needed.


Legacy KB System (APS) Data: RESL191933 V1.0, Originally authored by AlCh on 06/04/2008, Last Edited by AlCh on 06/04/2008
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?