Technical FAQs

Ask a Question

Are administrative rights required to run Unity Pro once it has been installed?

No, running Unity Pro does not require administrative rights. This is required only for the installation.


Legacy KB System (APS) Data: RESL191876 V1.0, Originally authored by DaSo on 07/01/2008, Last Edited by DaSo on 07/01/2008
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?