Technical FAQs

Ask a Question

Is there a way to prevent the Unity Pro Modbus Driver from automatically launching when the PC is rebooted?

Go to <Start><Run> and type: Na_config
Expand 'Modbus'
Highlight 'Modbus01'
Uncheck 'Autostart'.

 
Was this helpful?
What can we do to improve the information ?