Technical FAQs

Ask a Question

Can the SD memory card in a Modicon M340 CPU be removed while powered up?

The M340 does not have to be powered down but the SD memory card has to be stopped first before removing. The SD card is stopped by toggling system bit 65 (%S65) from off (0) to on (1). When the card is stopped, the green LED indicator below the memory card door will turn off. Now the SD card can be removed. If this LED is flashing it indicates that the card is being accessed. Also there is a SD memory card symbol in the status bar (lower right corner) which indicates yellow when there is a mismatch between PLC memory and SD card. A red symbol indicates wrong or missing SD card.


Legacy KB System (APS) Data: RESL191681 V1.0, Originally authored by DaSo on 04/15/2008, Last Edited by DaSo on 04/15/2008
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?