Technical FAQs

Ask a Question

How to show the PCFL functions name in the logic printout.

Goals and Symptoms

How to show the PCFL functions name in the logic printout.

Facts and Changes

ProWORx 32 version 2.1B

Causes and Fixes

If you provide a descriptor for the constant number that is associated with the PCFL block type
(i.e., KPID), it will get displayed on the network.

To accomplish this,

  • Right click on the logic window and select 'Properties'

 
  • Click on the 'View 1' tab (this view is used because only View 1 properties apply to the printout.)
  • Select 'Descriptor1' as shown below.
  • Click 'Apply'
  • Click 'OK' to close the 'Properties' window.

 
  • Click on the top node of the block and the constant number will appear in the 'Documentation' winodw.


  • Type in the name of the block (i.e., AIN) for the first line of the descriptor.


 
  • Click on the Logic window to apply the changes and you will see the name of the PCFL function appear.

Legacy KB System (APS) Data: RESL191551 V1.0, Originally authored by AlCh on 04/10/2008, Last Edited by AlCh on 04/10/2008
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?