Technical FAQs

Ask a Question

Recommendation on RAM extension size for Modular iPC

As most usual PCs, when RAM extension are used in the iPC, both RAM memories must have the same size: either 2*512 Mb or 2*1 Gb.


Legacy KB System (APS) Data: RESL191487 V1.0, Originally authored by ArGr on 03/22/2008, Last Edited by ArGr on 03/22/2008
Related ranges: Magelis Modular iPC
Was this helpful?
What can we do to improve the information ?