Technical FAQs

Ask a Question

How do I setup and save the router and subnet mask addresses on a Momentum 170ENT11002 communication module?

Goals and Symptoms

How do I setup and save the router and subnet mask addresses on a Momentum 170ENT11002 communication module?

Causes and Fixes

Due to the fact that the Momentum 170ENT11000 and 170ENT11002 communication modules do not have web pages to configure and save the IP information the bootp lite application must be used.


Above you will find an example with the proper syntax for assigning the static IP address, router IP address and subnet mask within bootp lite.

Attachments

(Removed File URL: 191400_51AA/bootplt.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/21a788c490581633c12574080058021f/fl_block_5/0.540?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL191400 V1.0, Originally authored by MiMe on 03/10/2008, Last Edited by MiMe on 03/10/2008
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?