Technical FAQs

Ask a Question

Twidoport to has 45 second time delay on startup when connected to an XTBG-G terminal.

Goals and Symptoms

Twidoport to has 45 second time delay on startup when connected to an XTBG-G terminal.

Facts and Changes

499TWD01100

Causes and Fixes


The Twidoport could appear to take up to 45 seconds to startup when it's connection state is
monitored in a connected Magelis XTB-G display terminal that is started at the same time.

If this happens:

  • Disable the option 'Check Project Integrity' in the 'Vijeo Designer' properties inspector
window for the 'XBT-G' terminal configuration.
  • Increase the 'StartupDelay' to 5 seoncds or more.

Note: There is nothing wrong with the 499TWD01100. The problem is only related to the
XBT-G terminal startup.



Legacy KB System (APS) Data: RESL191378 V1.0, Originally authored by AlCh on 03/06/2008, Last Edited by AlCh on 03/06/2008
Related ranges: ConneXview
Was this helpful?
What can we do to improve the information ?