Technical FAQs

Ask a Question

How to change the instruction toolbar used to add a logic element

Goals and Symptoms

How to change the instruction toolbar that is used to add a logic element

Facts and Changes

All versions of ProWORX 32

Causes and Fixes

The following procedure can be used to change the instruction toolbar that is used to add a logic element.

  • Right click on the Logic window and select 'Logic Properties'.
  •  

  • Click on the 'Environment' tab.
  • Use the arrow buttons next to the 'Button Number' textbox, select the number of the
'Instruction Toolbar' icon that is to be changed (i.e., 6)
  • Type in the text for the button. (The text must match the actual acronym that is used for the element.)




Click on the 'Apply' button.



 

Legacy KB System (APS) Data: RESL191362 V1.0, Originally authored by AlCh on 03/05/2008, Last Edited by AlCh on 03/05/2008
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?