Technical FAQs

Ask a Question

How to migrate an XBTL application from XBTP to XBTN/R

Goals and Symptoms

How to migrate an XBTL application from XBTP to XBTN/R

Facts and Changes

Most of the XBTP application run fine when migrated into XBTN/R. Though, it exists few limitations.

Causes and Fixes


******************************************
A/ Case of conversion of XBTP to XBTN/R
*************************************************

A1/ ESC touch function
XBTP: when you are in a page and you came here without using a link to page, then pressing on ESC does nothing.
XBTR: pressing on ESC causes to go back to the previous page, or to the default page.

Consequently: the PLC program needs to take in account this difference.

A2/ alarms historical
The display of alarmhistorical occurs differently
- XBTP : history is simply displayed
- XBTN/R: you need to enter to the alarm to display the history

A3/ Function touch:
XBTP: while a F touch is maintained pressed, the rest of the keyboard remains active
XBTN/R: while a F touch is maintained pressed, the rest of the keyboard remains inactive

A4/ Image of function keys
- For the XBT-H/P/E range, when a function key is linked to a page access, the corresponding bit of the "image of function keys" word is set to 1.
- For the XBT-N/R range, when a function key is linked to a page access, the corresponding bit of the "image of function keys" word keeps unchanged.

***************************************************************************
B/ Case of conversion of XBTP terminal with printer port to XBTR
****************************************************************

Conversion from XBTP022110 to XBTR411

For XBTP applications using printer function, the customers must take in account the following:

B1/ XBTRs don't support as many protocols as XBTPs.
From version XBTL V4.50, the supported protocols are :
- Modbus
- Modbus Slave
- Unitelway
- PPI
- DH485
- Sysmacway
- DF1
(+ MTFX :but this one doesn't exist on XBTP)

B2/ XBTR cannot support form pages.

B3/ The function of the dialog table "free format print table" is not supported on XBTR.


B4/ Steps for conversion
Finaly, the main steps with XBTL1000 to convert an application from XBTP to XBTR should be:

1/ remove all form pages from XBTP application
2/ IF the protocol of XBTP application exist with XBTR application
THEN replace the terminal type for XBTP by the terminal type for XBTN
ELSE
- change the protocol by selecting a new protocol
- change the terminal type
END


Legacy KB System (APS) Data: RESL191098 V3.0, Originally authored by DaBr on 02/25/2008, Last Edited by DaBr on 10/07/2008
Related ranges: XBT L1000, Magelis XBT H, XBT P, XBT E, Magelis XBT N, R, RT
Was this helpful?
What can we do to improve the information ?