Technical FAQs

Ask a Question

STBNIP2212 Web Page Applets Cannot be Viewed Using Microsofts Web Browser Internet Explorer 7

Goals and Symptoms

The purpose of this Resolution is to inform users that a problem exists when viewing STBNIP2212 web page applets using Internet Explorer 7 browsers as shown in the example below. The browser will display an X in the corner of a blank box where the applet would be.

 

Causes and Fixes

To resolve the web page applet issue using IE7, upgrade the STNIP2212 Ethernet NIM Exec to a version 2.30 or greater.


Legacy KB System (APS) Data: RESL191012 V1.0, Originally authored by DaDz on 02/07/2008, Last Edited by DaDz on 02/07/2008
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?