Technical FAQs

Ask a Question

UnityPro Simulator and function codes for HMI

Goals and Symptoms

If you connect any HMI to the Simulator of UnityPro you have only access to the %MW, Functioncodes: 3,6,16)

Facts and Changes

All UnityPro Versions up to V3.1

Causes and Fixes

With UnityPro V4.0 is planned to make all needed Function codes 1..6, 15 and 16 available. Then you have also access to 0x, 1x, 3x and 4x registers (Types in Unity %Mx, %Ix, %IWx and %MWx).


Legacy KB System (APS) Data: RESL190935 V1.0, Originally authored by KlSP on 02/04/2008, Last Edited by KlSP on 02/04/2008
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?