Technical FAQs

Ask a Question

Can I flash the Twido Exec with a USB programming cable?

Yes, you can flash the Twido Executive using a USB programming cable. The two USB programming options are: TSXCUSB485 converter with a TSXCRJMD25 or a TSXPCX3030 cable (no longer sold).


Was this helpful?
What can we do to improve the information ?