Technical FAQs

Ask a Question

How To Completely remove the 'Advantys Configuration Software' from the PC.

Goals and Symptoms

How To Completely remove the 'Advantys Configuration Software' from the PC.

Facts and Changes

All versions of 'Advantys Configuration Software'.

Causes and Fixes


The uninstallation of any software in Microsoft Windows does not completely delete all remnants
of the software. There is always some registry componnent that does not get uninstalled. This is also
true for 'Advantys Configuration Software'. The following procedure can be used to completely
uninstall 'Advantys Configuration Software'. and return the Windows registry back to the state that it was
in prior to installing 'Advantys Configuration Software'.

  • Open Internet Explorer and go to www.resplendence.com
  • Click on the 'Free Download' button.

 
  • Download the Registrar Registry Manager and install it to your PC.
  • Launch the Registrar Registry Manager.
  • Click on the 'Continue with LITE' button to use the demo version of the shareware.



WARNING: BE VERY CAREFUL WHEN USING THIS SHAREWARE TOOL TO EDIT THE
REGUSTRY. IF THESE STEPS ARE NOT FOLLOWED EXACTLY, YOU MAY
INADVERTENTLY DELETE SOMETHING ELSE WHICH CAN CORRUPT YOUR
WINDOWS OPERATING SYSTEM. SCHNEIDER ELECTRIC CANNOT BE HELD
RESPONSIBLE IF THESE DIRECTIONS ARE NOT FOLLOWED EXACTLY.
 
  • Click on the search icon.

 
  • Type in the word 'Advantys' in the 'Text or data to search for' textbox.
  • Type in or select the word 'registry' for the 'Where to search' textbox.

 
  • Click on the 'search' icon located at the lower left corner of the 'Advanced' search window.

 
  • Use the mouse to highlight all of the found entries.
  • Right-click and select 'Delete selected registry keys and values.


 

Legacy KB System (APS) Data: RESL190727 V1.0, Originally authored by AlCh on 01/21/2008, Last Edited by AlCh on 01/21/2008
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?