Technical FAQs

Ask a Question

How do I determine what type of licensing is on my USB dongle in Vijeo Citect?

Open Vijeo Citect Explorer. Under the Help menu select Citect Key Update. Once the Citect Key Update window is open, click on the Update Key button. The window will now list the licenses that are on the USB dongle.

Legacy KB System (APS) Data: RESL190498 V3.0, Originally authored by RoAl on 12/29/2007, Last Edited by GeMc on 05/02/2013
Related ranges: Vijeo Citect
Was this helpful?
What can we do to improve the information ?