Technical FAQs

Ask a Question

Will the 140NWM10000 work with Proworx32?

The Proworx32 programming software is not supported in the FactoryCast HMI Configurator that is used to configure the 140NWM10000 module.
To implement a FactoryCast HMI application, you need to configure the module in one of the supported software workshop (i.e. Unity Pro, Concept or PL7).


Legacy KB System (APS) Data: RESL190446 V1.0, Originally authored by MiMe on 12/21/2007, Last Edited by MiMe on 12/21/2007
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?