Technical FAQs

Ask a Question

What is the maximum number of devices a M340 BMX NOE 0100 can IO Scan?

The I/O Scanner on the BMX NOE 0100 module is limited to:
.. max. number of devices: 64


Legacy KB System (APS) Data: RESL190441 V1.0, Originally authored by MiMe on 12/21/2007, Last Edited by MiMe on 12/21/2007
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?