Technical FAQs

Ask a Question

What is the maximum exchange capacity of the IO Scanner serviceon the M340 NOE0100 module

For the BMX NOE 0100, the maximum IO Scanner exchange capacity of the M340 is the following:
.. read zone: 2048 words
.. write zone: 2048 words


Legacy KB System (APS) Data: RESL190440 V1.0, Originally authored by MiMe on 12/21/2007, Last Edited by MiMe on 12/21/2007
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?