Technical FAQs

Ask a Question

What is the maximum number of Ethernet connections for the BMX NOE 0100 Ethernet interface?

The BMX NOE 0100 module allows a maximum of the following type of Ethernet connections:
.. servers (32 connections)
.. clients (16 connections)
.. Transparent Device Access (2 connections)
.. scan up to a maximum of 64 devices using the I/O Scanner
.. serve as the address server for a maximum of 64 devices

 
Was this helpful?
What can we do to improve the information ?