Technical FAQs

Ask a Question

What is the maximum number of Ethernet connections for the BMX P34 20xx CPU Ethernet interface?

The BMX P34 20xx CPU module allows a maximum of the following type of Ethernet connections:
.. servers (32 connections)
.. clients (16 connections)
.. Transparent Device Access (2 connections)


Legacy KB System (APS) Data: RESL190437 V1.0, Originally authored by MiMe on 12/21/2007, Last Edited by MiMe on 12/21/2007
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?