Technical FAQs

Ask a Question

What would cause a "Parsing error: Invalid operation" when programming a Equation Network using ProWORX Nxt?

The most common cause of this error is when you enter the colon ":" after the result register. Chapter 8 of the Modicon Ladder Logic Block Library User Guide (840USE10100) states that the content of the Equation Network is in the form: "result := algebraic expression". Unlike Modsoft, ProWORX Nxt automatically inserts the colon ":" after the result register.
Below is a example of entering a colon ":" when programming a Equation Network with ProWORX Nxt and selecting the "OK" button:



Below is a example after removing the colon ":" when programming a Equation Network with ProWORX Nxt and selecting the "OK" button"
(It was accepted):


Legacy KB System (APS) Data: RESL1903 V1.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?