Technical FAQs

Ask a Question

What is new with Vijeo Citect V7.0?


§ The migration tool: A tool to assist in migrating version 6.1 projects to version 7.0

§ Clustering allows you to group different sets of the runtime components within a single project, allowing multiple independent systems to be monitored and controlled

§ Local variables: - replace memory PLC tags and allow you to store data in memory when you start your runtime system

§ Memory and Persist Modes A memory mode device retains values in memory, a persist mode device stores the value of each variable on a hard disk

§ Online changes version 7.0 supports live changes to I/O communications, tags, alarms, trends, reports, and graphics without needing to restart client applications

§ Publisher-Subscriber Data Acquisition Model Clients now subscribe to tags and receive notifications when values change. This enables event driven functionality rather than the need of constant polling.

§ Project- Based Network Configuration Network topology and configuration is now defined in the project rather than in the citect.ini configuration file.

§ SpeedLink Provides the ability to generate and link Vijeo Citect alarm, trend, and memory mode tags from Unity Pro database.

§ Web Gate Allows you to display remote Vijeo Designer Operator screens within Vijeo Citect.


Legacy KB System (APS) Data: RESL189787 V1.0, Originally authored by MiMe on 11/28/2007, Last Edited by MiMe on 11/28/2007
Related ranges: Vijeo Citect
Was this helpful?
What can we do to improve the information ?