Technical FAQs

Ask a Question

170AEC92000 High Speed Counter with 170FNT11001 FIPIO Communication Adapter Is Not Supported With a Premium on FIPIO Network

Goals and Symptoms

The purpose of this resolution is to inform users of Premium PLC's and PL7 or Unity Programming software that the Momentum High Speed counter is not supported on FIPIO.

Causes and Fixes

The 170AEC92000 High Speed Counter, when mounted with a 170FNT11001 FIP I/O Communication Adapter, is not supported because it cannot be configured using Unity or PL7 programming software in Debug Mode. It was decided by Marketing in August of 2007 that this issue would not be resolved. (Reference DMDI 1716E)


Legacy KB System (APS) Data: RESL189276 V1.0, Originally authored by DaDz on 11/17/2007, Last Edited by DaDz on 11/17/2007
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?