Technical FAQs

Ask a Question

Does Modsoft have password protection capability?

Modsoft does not have password protection capability but it does have the ability to assign a User Access Level. The User Access Level can be assigned by using the Modsoft Command Line Switch /Ln where the number "n" sets the default User Access Level. This is a number between 0 and 8. Each incremental increase includes all privileges of the levels below it.
0 Allows monitoring only.
1 RDE Online Changes.
2 Allows PLC to File transfer.
3 Allows PLC Start, Stop
4 Allows File to PLC transfer.
5 Save Programs, Offline editors.
6 Allows Full Programming.
7 Same as Level 6.
8 Allows Executive Downloads.

Example: Modsoft /L4 sets the User Access Level to 4.


Legacy KB System (APS) Data: RESL1891 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modsoft
Was this helpful?
What can we do to improve the information ?