Technical FAQs

Ask a Question

Why am I not able to generate PID trace when using Ethernet connection to a Twido PLC?

If your Twido PLC has a firmware lower than 4.10 you will not be able to generate a PID trace via the Ethernet port. To update your Twido firmware use the attached file.
Twido_Firmware_V4_10.zip


Legacy KB System (APS) Data: RESL188680 V1.0, Originally authored by TVe on 10/27/2007, Last Edited by TVe on 10/27/2007
Related ranges: TwidoSuite, Twido Soft
Was this helpful?
What can we do to improve the information ?