Technical FAQs

Ask a Question

In Twido PLC, why would an internal coil (%M) maintain its state after a power cycle? Is there a way to prevent this?

The internal memory bits do not reset after a power cycle. The following logic may be used to reset all internal memory bits:


Legacy KB System (APS) Data: RESL188665 V1.0, Originally authored by TVe on 10/27/2007, Last Edited by TVe on 10/27/2007
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?