Technical FAQs

Ask a Question

Substitution for XUEF10031.

Goals and Symptoms

Substitution for XUEF10031.

Facts and Changes

XUEF10031
replacement, substitution

Causes and Fixes

The substitution for XUEF10031 is XUX0ARCTT16. If a mounting accessory is required, XUZX2000 can be used. The advised reflector is XUZC50.


Legacy KB System (APS) Data: RESL188614 V1.0, Originally authored by FrDa on 10/25/2007, Last Edited by FrDa on 10/25/2007
Related ranges: Osiris
Was this helpful?
What can we do to improve the information ?