Technical FAQs

Ask a Question

What is the difference between the Quantum 140DAO84010 and 140DAO84210 modules?

They are both Quantum AC output modules. The difference is the voltage and grouping.
140DAO84010.....24-115 VAC, 16 isolated channels.
140DAO84210.....100-230 VAC, 4x4 grouped channels.


Legacy KB System (APS) Data: RESL188417 V1.0, Originally authored by RoAl on 10/11/2007, Last Edited by RoAl on 10/11/2007
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?