Technical FAQs

Ask a Question

Which controllers does the P190 Programmer support?

The P190 Programmer is used to program 184/384, 484, 584, 884, 984, and Micro 84 Programmable Controllers along with the 2184 Motion Controller.


Legacy KB System (APS) Data: RESL187948 V1.0, Originally authored by RoAl on 09/08/2007, Last Edited by RoAl on 09/08/2007
Related ranges: Compact
Was this helpful?
What can we do to improve the information ?