Technical FAQs

Ask a Question

What are the part#'s for the Panelmate Plus Modbus Plus Interface Board?

The part #'s for the Panelmate Plus Modbus Plus Interface Boards are:
1) MM-PMMP001C - Panelmate Plus 2000 / 3000 / 4000 Modbus Plus Interface, CE
2) MM-PMMP002C - Panelmate Plus 2000 / 3000 / 4000, Dual MB+ Interface, CE
3) MM-PMMP003C - Panelmate Plus 1000 / 1500 Modbus Plus Interface, CE


Legacy KB System (APS) Data: RESL1877 V1.0, Originally authored by on , Last Edited by on
Related ranges: Panelmate
Was this helpful?
What can we do to improve the information ?