Technical FAQs

Ask a Question

What are the minimum operating system requirements to run the M340 UnityLoader version 1.0 software?

System: Pentium processor 500 MHz or higher
RAM memory: 256 MB
Hard disk space: 25 MB including the memory space for the software installation, temporary space for execution.
Operating System: Windows 2000 or Windows XP


Legacy KB System (APS) Data: RESL187652 V1.0, Originally authored by MiMe on 08/20/2007, Last Edited by MiMe on 08/20/2007
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?