Technical FAQs

Ask a Question

What causes an 'error opening database, error 1' when importing a file into the ProWORX 32 Schneider Alliance tool?

This error can occur if the .SAF file's 'read only' attribute is checked.


Legacy KB System (APS) Data: RESL187458 V1.0, Originally authored by DaSo on 02/20/2009, Last Edited by DaSo on 02/20/2009
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?